AXIS#.VL.FB

Description

AXIS#.VL.FB returns the velocity feedback as it is received in the velocity loop after passing through Filter 3 and Filter 4.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Depends on AXIS#.UNIT.VROTARY

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Range

N/A

Default Value

N/A

Data Type

Float
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
AXIS1.VL.FB

606ch

00h

Signed32

Velocity

-

Read only

Yes

AXIS2.VL.FB

686ch

00h

Signed32

Velocity

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.FB

6024

1788

Signed32

Read Only

Velocity

AXIS2.VL.FB

71560

1178

Signed32

Read Only

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.FB

6024

Float

Read Only

Velocity

Related Topics

"Velocity Loop"